Trace Data dialog box (XY Plot)
How do I open the Trace Data dialog box?
On the plot surface, right-click a trace and select
Trace Data
.You can view trace data for a specific period of time, and can organize it for printing. The following options are available:
Option | Description |
|---|---|
Time period | Select a time period for which you want to display trace data. |
Narrow/ Wide/ Sparse Wide | Choose one of the following:
|
Print across pages | Select this check box to horizontally print trace data across multiple pages. |
You can click one of the following options:
- Print Previewto preview the list before sending it to the printer.
- Printto print the list.
- Saveto save the list to either a comma or tab delimited file.
Provide Feedback