Retrieval page - Sampling tab (XY Plot)
How do I open the Sampling
tab in the Change Settings dialog box?
- On theRetrievalproperties page, clickChange.
- In theChange Settingsdialog box, click theSamplingtab.
Data sampling determines the method used to select and analyze a subset of data. You can customize sampling options for retrieving data on this dialog box.
The following options are available:
Setting | Description |
|---|---|
Select a sampling type | Select a data sampling method to use. |
Sampling method | Select one of the following options:
|
Provide Feedback