Retrieval page - General tab (XY Plot)
How do I open the General
tab in the Change Settings dialog box?
- On theRetrievalproperties page, clickChange.
- In theChange Settingsdialog box, click theGeneraltab.
The first time you select the
Custom
retrieval mode on the Retrieval
tab, the Change Settings
dialog box opens. You can also change custom settings after the initial configuration by clicking Change
.The following options are available:
Setting | Description |
|---|---|
Deadbands | Use one of the following options to limit the number of rows returned by the function.
|
Quality | Uses the standard quality property stored with a tag on most historians to determine whether results are returned. |
Advanced | Sets a maximum number of rows to return.
|
Version | Retrieves the latest data values or the original values stored with the item. |
Provide Feedback