Use x-axis cursors (TrendPro)
When the x cursor is enabled, two vertical cursors that slide along the x-axis display. Each cursor can be operated individually. You can also use the x-axis cursor with the y-axis cursor. This feature is useful when you stack the y-axis so you can quickly see the values for a point in time for all traces at once and compare those values.
Cursors:
- Can be used while zooming in on data.
- Allow panning of data.
- Display values of data points that touch the cursor.
- Calculate the time difference between cursor data points.
To use x-axis cursors
- On the TrendPro toolbar, clickX-axis Cursors
. Two vertical cursors display on the trend. - Drag each cursor left or right on the plot surface. The following information displays:
- Data point values for each trace at the cursor location.
- Date and time display for each cursor location.
- Time difference has been calculated along the x-axis and displays between the two cursors.
Provide Feedback