Traces page (TrendPro)
How do I open the Traces
page (Properties dialog box)?
- On thePropertiesdialog box, click theTracestab.
- Click the tag name in the left pane.
- Click theTraceradio button.
Trace properties allow you to configure whether statistics are calculated for a trace, the format for numeric, discrete, and time tags, and other options for the current trend. The properties are applied immediately to the current trend.
TIP:
You can add a new trace or a parameter to the trend by clicking
. Parameters accept a format of #
. Parameters accept a format of #number
, such as #1.The following options are available:
Property | Description |
|---|---|
Trace | The options for the trace. Select from the following:
|
Style | The options that define the style of the trace, such as line color. Select from the following:
|
Display | The options that display on the plot. Select from the following:
|
Point markers | The shape, color, and size of points on the trace. |
Numeric tags | The options that apply to numeric tags. Select from the following options:
|
Plotting algorithm | The type of interpolation that is applied to the plot. Select one of the following options:
|
Discrete and time tags | The options that apply to discrete and time tags. Select from the following options:
|
Provide Feedback