X-Axis page (TrendPro)
How do I open the X-Axis
page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- In the left pane, clickX-Axis.
X-axis properties allow you to define how the x-axis displays time in the current trend. The properties are applied immediately to the current trend.
TIP:
You can add a new trace or a parameter to the trend by clicking
. Parameters accept a format of #
. Parameters accept a format of #number
, such as #1.The following options are available:
Property | Description |
|---|---|
Label | The option to include in the axis label. Click the Use default text checkbox to display the default time period as the label. Enter custom text after clearing the Use default text checkbox. |
Axis | The display options for the axis. Select from the following options:
|
Time axis mode | The mode used to display time periods. Select one of the following options:
|
Tick marks | Specifies short lines along the axis line that specify value divisions. Select one of the following options:
|
Provide Feedback