Live Data page (TrendPro)
How do I open the Live Data page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- ClickLive Datain the left pane.
Live Data properties store live data in a buffer so it can be retrieved at a later time for the current trend. The following properties are applied immediately to the current trend.
The following options are available:
Property | Description |
|---|---|
Collector | The options to store live data for later use. Select from the following options:
|
Provide Feedback