Automatically scale trends
When creating new trends, automatic scaling determines a scale for the y-axis that will best display the available data. Trend evaluates the trace data values and sets the y-axis values based on the minimum and maximum data values to display.
To automatically scale a trend
- On theTrendProtoolbar, clickAutomatic Scales
.TIP:If you have manually defined Min/Max values for any tags in the trend, enabling automatic scaling will remove those values.
Provide Feedback