Toolbar commands
The following table shows the commands on the toolbar of the
Edit
tab.Commands | Description |
|---|---|
Create ![]() | Select this icon to create a recipe. Each recipe must have a unique name. When you create a recipe, you define the ingredients that make up the recipe, whether they are number or string type, what the data values for each ingredient will be, and what tag each value will be written to. |
Duplicate ![]() | Select this icon to duplicate an existing recipe. |
Delete ![]() | Select this icon to delete a recipe. |
Save ![]() | Select this icon to save changes for a recipe. |
Refresh ![]() | Select this icon to refresh the current and preset values of tags associated with the ingredient and show them in the recipe edit table. If the current values are different from the preset values, the current values are displayed in red. |
Upload ![]() | Select this icon to read the tag values from the location specified in the tag set of the recipe file and save those values to the recipe. Note: The uploading stops if an error occurs, but the system continues to validate the recipe file and logs the error messages to FactoryTalk Diagnostics. It may take some time if a large number of errors occurs. During that time, you may have a slow response if using the RecipePro+ editor. To avoid this, use the RecipePro+ editor when the FactoryTalk Diagnostics logging completes. |
Upload and create ![]() | Select this icon to read the tag values from the location specified in the tag set of the recipe file and save those values to a new recipe. The new recipe is duplicated from the recipe selected. |
Download ![]() | Select this icon to write the ingredient values of the specified recipe file to the tags in the tag set. By default, only tags that are accessible will be downloaded. To check whether all tags are accessible before downloading, select Check communication before download . If one or more tags are not accessible, the download command will not be executed. |
Provide Feedback