Required security permissions
Users or groups must be granted with the appropriate security permissions to perform certain actions in the RecipePro+ editor. You can set the security permissions on the and expand it.
Permissions
tab. To view the permissions, in the Security Settings
dialog box, navigate to FactoryTalk View SE
TIP:
To open the dialog box, in the
FactoryTalk View Studio
Explorer window, right-click the appropriate application or area and select Security
.Because security settings are inherited down the tree, choose the application or area at the highest possible level in the tree. For example, if you apply security settings at an application level, those settings apply to all of the areas within that application. If you apply security settings to a particular area, the settings apply to only that area and to other areas contained within that area.
To operate recipes in the RecipePro+ editor, users or groups must have at least the
RecipePro: Preview
permission. Otherwise, the recipes will not be visible in the editor.
TIP:
The
RecipePro: Preview
permission is specifically designed for FactoryTalk ViewPoint
mobile users. If you want to restrict certain users to view and access the recipes on mobile devices, you must deny this permission for those users.The following table shows additional security permissions required for certain actions.
To do this | You need these additional security permissions |
|---|---|
Create a recipe | RecipePro: Create |
Delete a recipe | RecipePro: Delete |
Download a recipe | RecipePro: Download |
Duplicate a recipe | RecipePro: Create |
Edit a recipe | RecipePro: Edit |
Modify a tag set | RecipePro: Edit RecipePro: Modify TagSet |
Import a recipe | RecipePro: Create RecipePro: Edit RecipePro: Modify TagSet |
Rename a recipe | RecipePro: Edit |
Upload a recipe | RecipePro: Edit RecipePro: Upload |
Upload and create a recipe | RecipePro: Create RecipePro: Upload |
RecipeProDownload command | RecipePro: Download |
RecipeProUpload command | RecipePro: Edit RecipePro: Upload |
If you have secured HMI tags, the security codes are not validated at runtime. Users or groups that are not assigned the tags' security code are able to perform the download or upload operation.
Provide Feedback