Add client keys
Use the
Add Key
dialog box to define a new key or key sequence that can be used in the client application.The following table shows options in the dialog box.
Option | Description |
|---|---|
Key | Specifies the key used by the client application. |
Modifier | Specifies a modifier key that must also be pressed to perform the action. You can use more than one modifier per key. |
Provide Feedback