Reserved keys
In
FactoryTalk View
, some keys or key combinations have particular actions associated with them in the FactoryTalk View SE
Client or when you test running a graphic display. For this reason they are called reserved keys.If you create a display or an object key using a reserved key, the reserved key action is disabled because the display or object key action always takes precedence.
TIP:
If you create a client key using a reserved key, pressing the key will initiate client key and the reserved key actions. This can result in unpredictable behavior and is not recommended.
Reserved keys | Action |
|---|---|
"+" on numeric keypad | Displays the Recipe dialog box when the Recipe editor is highlighted, or saves the recipe if Ctrl+W was pressed previously, or restores the recipe if Ctrl+R was pressed previously. |
Backspace | Deletes the character to the left of the cursor. |
Delete | Deletes the character to the right of the cursor. |
Shift+End+Delete | Deletes everything from the cursor position to the end of the line. |
Home+Shift+End+Delete | Deletes the contents of the current input field. |
Enter |
|
Escape | Closes the Object Key menu, or exits the input mode of a continuously-updating input field. |
Home | Positions the cursor at the beginning of the data entry field. |
PgUp | Uploads data from all input fields. |
Ctrl+PgUp | Uploads data into the selected input field. |
PgDn | Downloads data from all input fields. |
Ctrl+PgDn | Downloads data from the selected input field. |
Tab | In a dialog box, moves the cursor to the next data entry field; in a graphic display, moves the focus to the object with the next highest index number. |
Shift+Tab | In a dialog box, moves the cursor to the previous data entry field; in a graphic display, moves the focus to the object with the next lowest index number. |
Left/Right Arrow | Moves the cursor one position left or right. |
Up/Down Arrow | Moves the selection bar on the Object Key menu. |
Ctrl+Up Arrow Ctrl+Left Arrow Ctrl+Down Arrow Ctrl+Right Arrow | Moves focus to an object in the direction in which the arrow points. |
Ctrl+R | Sets input focus to the recipe object and prepares for a recipe restore. |
Ctrl+W | Sets input focus to the recipe object and prepares for a recipe save. |
Ctrl+C Ctrl+Ins | Copies the selected items(s) to the clipboard. |
Ctrl+X Shift+Del | Cuts the selected items(s) and places them on the clipboard. |
Ctrl+V Shift+Ins | Pastes the contents of the clipboard at the current cursor position. |
Ctrl+F4 Ctrl+Shift+F4 | Closes the active window. |
Ctrl+F6 | Moves focus to the next window. |
Ctrl+Shift+F6 | Moves focus to the previous window. |
Provide Feedback