Button Properties - Action tab
The following table shows options in the
Action
tab.Options | Description |
|---|---|
Action | Click the down arrow to scroll the list of actions and select one. The action that you select determines which fields will be available in the tab.
|
Tag | This is displayed when any Action option except Run command, is chosen. Specify the path and name of the tag that will be the recipient of the action. |
Remark | This is displayed when the Action option is Toggle tag value . Enter a customized message that will be shown in the Diagnostic List when changing the tag's value at runtime. This is helpful for monitoring and identifying operations that change tag values among a large number of diagnostic messages.You can configure multiple languages for remark at design time. However, the remark message is only logged in the default language. For example, your application has three languages configured and the remark messages are also configured in those three languages. If the application's default language is English and the current language is Chinese, the remark messages are logged in the default language English. The following placeholders are available:
For example, a message for changing the automatic/manual mode of a water pump motor control circuit could be Changed water pump motor control circuit mode from /C to /N .If you want to switch the language of extended tag properties added by the Insert Tag option, use /L before the inserted tag without space.Tip : Semicolon (;) is FactoryTalk View SE 's reserved character. If you want to use the semicolon in the remark message, you must enclose it in double quotation marks. |
Press action | This field, and those that follow, are available when Run command is chosen as the button's action. Type the FactoryTalk View command to be executed when the mouse cursor is over the button and the mouse button is pressed down, or else click the browse button to open the Command wizard and use it to build a command string. |
Repeat action | Type the FactoryTalk View command to be executed when the mouse cursor is over the button and the mouse button is pressed and held down, or else click the browse button to open the Command wizard and use it to build a command string. The action is repeated at the rate specified by Repeat Rate as long as the mouse button is held down. |
Repeat rate (secs) | Type the rate in seconds at which the repeat action is to be executed. |
Release action | Type the FactoryTalk View command to be executed when the mouse cursor is over the button and the mouse button is released, or else click the browse button (...) to open the Command wizard and use it to build a command string. If no press or repeat action is specified, the release action occurs when the button is clicked (mouse button is pressed and released). |
Confirm and E-Signature settings | Select an option to configure the confirmation type before actions are performed.
|
Provide Feedback