Confirmation dialog box
Use the dialog box to configure how the confirmation pop-up dialog box will look like when
executing commands or actions on buttons, numeric inputs, string inputs, or objects with
touch animation.
The following table shows options in the dialog box.
Options | Description |
|---|---|
Title Bar | Select the check box to show the title bar of the confirmation dialog box. You can enter up to 255 characters. Click Insert Variable to add an embedded variable to the title bar. After you set up the embedded variable, the embedded variable syntax appears in the field but the text of the variable appears on the dialog box. |
Window position | Select a position where the conformation dialog box will be shown. |
Caption | Enter the message that will be shown in the confirmation dialog box. Click Insert Variable to add an embedded variable to the title bar. After you set up the embedded variable, the embedded variable syntax appears in the field but the text of the variable appears on the dialog box. |
Font | Select or enter a font for the message. |
Bold (B), Italic (I), Underline (U) | Click a letter, or letters, to specify the font style for the message, if required. |
Image settings | Choose a pattern and color for the confirmation dialog box. You can also import a bitmap or icon to be displayed on the dialog box.
|
Scale image | Select this check box to scale the image to fit within the dimensions of the dialog box. This applies to both referenced and imported images. The recommended dimensions are 48 x 48 pixels. |
Button settings | Select buttons that will be shown in the confirmation dialog box, including OK and Cancel , OK only , Yes and No , and Yes only . |
Provide Feedback