Create elements for controlling the max value
    Create a label and a gauge to control the maximum value.
- Create the maximum value label:- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the label, select, and enter MaxValueLabel. MaxValueLabel.
- InPropertiessetTexttoMaximum Value.
 
- Configure the max gauge:- InProject view, right-clickMainWindow (Type)and select .
- Hover-over the gauge, select, and enter MaxGauge. MaxGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback