Develop a constrained linear gauge
    Develop an interface that enables you to change the current value, max value, and minimum value of a variable.
 
    
     NOTE: 
    
Download a sample project:
 ConstrainedLinearGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.

Select  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
  to run the project using the client
        emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback