Keyboard shortcuts
    FactoryTalk Optix Studio
 supports these keyboard shortcuts.Global
            
  | Shortcut | Description | 
|---|---|
| F1 | Open  FactoryTalk OptixHelp. | 
| Ctrl C | Copy the selected item. | 
| Ctrl V | Paste the copied item into the selected location. | 
| Ctrl Z | Undo previous action. | 
| Ctrl Y | Redo previous action. | 
| Ctrl S | Save the current  FactoryTalk Optix Applicationproject. | 
| F5 | Run  FactoryTalk Optix Application. For more information, see Deploy a FactoryTalk Optix Application. | 
| Ctrl Shift F | Find text in the current project. For more information, see Find text in a project. | 
| Ctrl Shift H | Find and replace text in the current project. For more
                                information, see Replace text in a project. | 
| Delete | Delete the selected item. | 
| Esc | Discard edits or close a dialog. | 
| Alt Enter | Add a new line. | 
| Enter | Interact with the selected item. | 
Panes
            The following shortcuts apply to panes in 
FactoryTalk Optix Studio
. For more
                information about FactoryTalk Optix Studio
 panes, see FactoryTalk Optix Studio GUI.| Shortcut | Description | 
|---|---|
| Up arrow | Select previous item. | 
| Down arrow | Select next item. | 
| Right arrow | Expand the selected item. | 
| Left arrow | Collapse the selected item. | 
| Alt Left
                                arrow | Select the previously selected item in  Project
                                    view. For more information, see Project view. | 
| Alt Left
                                arrow | Select the next item in  Project view. For
                                more information, see Project view. | 
| Shift | Select all items between the selected item and the clicked
                                item. | 
| F2 | Rename the selected item. | 
Localization dictionary
            For more information about localization dictionaries and strings translation, see
                    Localization editor.
| Shortcut | Description | 
|---|---|
| Ctrl A | Select all keys and values in the translation table. | 
UI editor
            The following shortcuts apply to the editor that allows you to arrange graphic
                objects and create user interfaces for 
FactoryTalk Optix Applications
. For more
                information, see Editor.| Shortcut | Description | 
|---|---|
| Up arrow | Move the selected object up on the grid. | 
| Down arrow | Move the selected object down on the grid. | 
| Left arrow | Move the selected object left on the grid. | 
| Right arrow | Move the selected object right on the grid. | 
| Shift Up arrow | Move the selected object up and align the object to the
                                grid. | 
| Shift Down
                                arrow | Move the selected object down and align the object to the
                                grid. | 
| Shift Left
                                arrow | Move the selected object left and align the object to the
                                grid. | 
| Shift Right
                                arrow | Move the selected object right and align the object to the
                                grid. | 
Provide Feedback