Development and scripting FAQs
    How do I develop scripts in FactoryTalk Optix Studio? What languages are
                    supported?
You can develop NetLogic scripts in C# with the use of FactoryTalk Optix Studio and
                an external code editor to extend the functionalities of your FactoryTalk Optix
                projects. See Extending projects. 
Are there any NetLogic script examples available?
Yes, there are NetLogic script examples. See NetLogic tutorial.
Can I use external packages in my NetLogic scripts?
Yes, you can use external NuGet® packages in your NetLogic scripts. See NuGet packages.
To work with a specific firmware do I have to use a particular FactoryTalk Optix
                    version?
For firmware 6, you must use FactoryTalk Optix version 1.5 or greater.
Can I develop responsive UI with FactoryTalk Optix?
Yes, you can develop responsive UI with FactoryTalk Optix Studio. See Responsive user interface.
Where can I find and download FactoryTalk Optix application examples?
You can find and download FactoryTalk Optix Application examples in the FactoryTalk
                Optix Help. See Application examples. You can also find
                examples on the FactoryTalk Hub 
Resources
 page.What are the available communication drivers in FactoryTalk Optix?
You can check and learn about the available communication drivers in FactoryTalk
                Optix Help. See Communication drivers overview and Communication drivers.
Can I downgrade the firmware of an Optix Panel?
No, the only way to downgrade firmware of an Optix Panel is to perform a factory
                reset of the panel.
Provide Feedback