Configure idle timeout for a session
    Use 
IdleTimeoutEvent
 to have an idle timeout apply to the
      entire session. A timeout can trigger any custom event- InProject view, right-click theUIfolder and select .UISession# (type)appears inProject view.
- (optional) Hover-over theUISession# (type), selectand enter a new name for the UI session. 
- InProperties, set these values:- Inactivity timeout duration. Enter the duration for the timeout.
- Inactivity timeout active. Set toTrue.
 
- UnderEventsafterIdleTimeoutEvent, select Add new method, expandCommands, and select the command to execute when the timeout event is triggered. Add new method, expandCommands, and select the command to execute when the timeout event is triggered.
- Apply the session to presentation engines:- InProject view, select a presentation engine.
- InProperties, fromSessions, select the UI session type.
 For more information about presentation engines, see Presentation engines.
Provide Feedback