Troubleshoot upgraded projects
    If you encounter issues with upgraded projects, consider the following
            guidelines.
Projects upgraded to 1.6.0 or higher
            If you upgrade a project lower than 1.6.0 to 1.6.0 or higher, make sure to replace
                old unsupported properties with new properties in NetLogics:
  
    
| Old properties | New properties | 
|---|---|
| uint[] ParentArrayIndex | ElementAccess ParentElementAccess | 
| IUAVariable ParentArrayIndexVariable | IUAVariable
                                    ParentElementAccessVariable | 
Consider the following
                example:
[ExportMethod] public void ChangeParentScalarIndex() { IUAVariable arrayVar = Project.Current.GetVariable("Model/ArrayVar"); DynamicLink myDynamicLink = arrayVar.Children.Get<DynamicLink>("DynamicLink"); //-------------------- 1.4.X IMPLEMENTATION -------------------- //Accessing parent array index in FactoryTalk Optix version lower than 1.6.0. //You can use monodimensional and multidimensional arrays. uint[] myArrayIndex = { 3 }; myDynamicLink.ParentArrayIndex = myArrayIndex; //You can only use the `ParentScalarIndex` property with a monodimensional array. //The following simplifies the access to the parent array index with a scalar value. //The following implementation is equivalent to the previous implementation. myDynamicLink.ParentScalarIndex = 3; //------------------------------------------------------------ //-------------------- 1.6.X IMPLEMENTATION -------------------- //Accessing parent array index in FactoryTalk Optix version 1.6.0 and higher. //Create an `ElementAccess` wrapper structure that exposes `ArrayIndexes` and `FieldIndexes`. //Use `ArrayIndexes` for arrays; Use `FieldIndexes` for structures. //Manage the access to an array or structure with `ParentElementAccess`. ElementAccess myElementAccessStructure = new ElementAccess(myArrayIndex); myDynamicLink.ParentElementAccess = myElementAccessStructure; //------------------------------------------------------------ }
     TIP: 
    If errors about depreciated properties in scripts
                or widgets appear in the upgrade report, remove the impacted scripts or widgets from
                the project and add the scripts or widgets again. For more information, see Libraries.
troubleshooting
struct
upgrade
projects
uint[] ParentArrayIndex
IUAVariable ParentArrayIndexVariable
ElementAccess ParentElementAccess
IUAVariable ParentElementAccessVariable
        
Provide Feedback