Upgrade a project
    You can open a project that was created with a previous version of 
FactoryTalk Optix Studio
 with later a version by upgrading the project. During the upgrade, FactoryTalk Optix Studio
 creates a backup copy of the original version of the
      project.
     IMPORTANT: 
    After the upgrade, you can no longer open the
      project with the previous version of 
FactoryTalk Optix Studio
. To restore an
      incorrectly upgraded project, see Restore a project.- Open a project created with a previous version ofFactoryTalk Optix Studio.A message appears to request an upgrade of the modules in use.
- SelectUpgrade.A detailed report of the upgrade process appears.
- After reviewing the report, selectContinueto confirm that the project should be upgraded.
FactoryTalk Optix Studio
 upgrades and opens the project. In case of any issues, see Troubleshoot upgraded projects.upgrade
version
    
Provide Feedback