Smart Objects
    Ensure that the feature is set up. See Set up Smart Objects.
- To create instances of controllers, right-click theSmartObjectsfolder, and select: .If you have multiple controllers, you must create multiple instances.
- Define settings for the controller:- In theControllerFilePath, enter the file path to the controller.
- In theIPAddress, enter the IP address of the controller.
 
- Right-click the controller, and perform the following actions:- To read the Smart Objects model, execute theReadModelsmethod.New properties of SmartObjectImporter display, following the naming conventionTarget for. You can use these properties to defineso_model_nameFactoryTalk Optixmodel location for Sync object models.
- To move Smart Objects model to FTOptix model, execute theImportSmartObjectsmethod.Imported SmartObjectImporter models appear in the predefined location, following the naming conventionTarget for. You can use these properties to defineso_model_nameFactoryTalk Optixmodel location for Sync object models.
 
Provide Feedback