Configure and FTP client
    - Install stable versions of the following NuGet package: FluentFTP. See NuGet packages.
- Configure the requiredFTPClientLogicscript parameters. See FTP Client configuration.
- Run theFTPClientLogicscript.
Provide Feedback