Configure a transitioned event
    Trigger methods if the value of a variable or object property meets a specific condition.
- InProject view, select an object or a variable.
- InProperties, right-click a variable or a property and select .TIP: If needed, selectto add a variable. 
- InEvents, fromTransitionselect:- Equal to
- Not equal to
- Greater than
- Greater than or equal to
- Less than
- Less than or equal to
 
- Set theValueproperty.TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
- Next toVariableTransitioned, select. 
- Select a method:- For global methods, expandCommands.
- For local methods, expand the nodes that expose methods (for example, aDataGridnode exposes aRefreshmethod), or expand the node related to a specific NetLogic.
 
- (optional) If the method requires arguments, expand the method and set arguments.
meet condition
transition event
    
Provide Feedback