Expression evaluator
    Calculate the result of an expression with integers, decimals, numeric variables, string variables for string comparisons, arithmetic and Boolean operators, or a set of functions.
Properties
      
  | Property | Description | 
|---|---|
| Expression | The expression to be calculated. To add variables to the expression, enter consecutive numbers or unique strings
                  starting with  #in braces {}. For example, enter {0}and then enter {1}later in the
                  expression. Fill {#}Dynamic link The expression can contain an unlimited number of correctly opened and closed
                  braces  {}. If the expression does not follow the correct syntax,
                  the converter does not perform the calculation. | 
| Mode | The direction of the dynamic link:
         
 | 
Source
      One or more variables identified by:
          
- {placeholderindex_number}
- Progressive integer equal to or greater than zero. For example,{1}
- {#placeholderplaceholder_identifier}
- String prefixed with#. For example,{#speed}
     TIP: 
    Use any combination of placeholders in any order. Use any number of placeholders in the expression.
Literals
      - Boolean.
- Integers.
- Decimals where the decimal separator must be a point.
- Hexadecimal numbers with the prefix0x.
- Text such as a string delimited by double quotation marks.TIP: Double quotation marks repeated twice ("") are interpreted as an escape sequence.
- Date and time. For example,2017-06-28T15:26:06.0790910.
Operators
      
  | Category | Operator | Associativity | Comments | 
|---|---|---|---|
| Unary | Unary minus:  - Bitwise NOT:  ~ Cast operator:  (type) | Right to left | The cast operator  (type)applies to all numeric data types and Boolean only. | 
| Multiplicative | *, /, % | Left to right | |
| Additive | +, - | Left to right | |
| Shift | <<, >> | Left to right | Shift and Relational operators apply to these data types:
                   
 | 
| Relational | <, <=, >, >= | Left to right | |
| Equality | ==, != | Left to right | Equality operators apply to these data types:
                   
 | 
| Bitwise AND, XOR, OR | &, ^, | | Left to right | |
| Logical AND | && | Left to right | |
| Logical OR | || | Left to right | 
Data types
      Data type conventions in the expression evaluator:
        
- Literal integers are Int32.
- Decimal literals are Double.
- Numerical values are considered to be Int32.
- Literals true and false are interpreted as Boolean.
- The / operator always returns a Double value.
- The % operator generates an exception when there is division by modulo zero.
- The % operator accepts Float and Double operands.
- All functions return a Double value except for sign, which returns an Int32 value.
The 
type
 of unary cast operators can be of these data types:
        - bool, Boolean
- sbyte, SByte
- short, Int16
- int, Int32
- long, Int64
- byte, Byte
- ushort, UInt16
- uint, UInt32
- ulong, UInt64
- float, Float
- double, Double
Operators applied to specific data types:
        
  
    
| Operator | Operand1 | Operand2 | Description | 
|---|---|---|---|
| Plus | DateTime | Integral number | Operand2is interpreted as milliseconds. | 
| Plus | Integral number | DateTime | Operand1is interpreted as milliseconds. | 
| Plus | DateTime | TimeZone (Struct) | Operand2is interpreted as minutes (TimeZone.Offset). | 
| Plus | TimeZone (Struct) | DateTime | Operand1is interpreted as minutes (TimeZone.Offset). | 
| Plus | TimeZone | Integral number | Operand1is interpreted as minutes (TimeZone.Offset). Operand2is interpreted as minutes. | 
| Plus | Integral number | TimeZone | Operand1is interpreted as minutes. Operand2is interpreted as minutes (TimeZone.Offset). | 
| Minus | DateTime | Integral number | Operand2is interpreted as milliseconds. | 
| Minus | DateTime | TimeZone (Struct) | Operand2is interpreted as minutes (TimeZone.Offset). | 
| Minus | TimeZone | Integral number | Operand1is interpreted as minutes (TimeZone.Offset). Operand2is interpreted as minutes. | 
Functions
      Functions for use in the expression evaluator:
        
  
    
| Function | Syntax | Description | Return data type | 
|---|---|---|---|
| max | max( value1, value2, value3, ...) | Returns the greatest value. | Double | 
| min | min( value1, value2, value3, ...) | Returns the lowest value. | Double | 
| avg | avg( value1, value2, value3, ...) | Returns the average of the given values. | Double | 
| abs | abs( value) | Returns the absolute value of the given number. | Double | 
| trunc | trunc( value) | Returns the integer part of a decimal number. | Double | 
| ceil | ceil( value) | Returns the approximated value by excess. | Double | 
| floor | floor( value) | Returns the approximated value by defect. | Double | 
| round | round( value) | Returns the approximation to the nearest integer. | Double | 
| sqrt | sqrt( value) | Returns the square root of the given number. | Double | 
| sign | sign( value) | Checks if the given floating point number is negative. Returns  0if true or 1if false. | Int32 | 
| like | like( string_value, pattern) | Applies only to String, QualifiedName, and LocalizedText data types. Returns  trueif the string_value parameter matches the pattern. The  patternaccepts the %wildcard at the beginning or at the end. Examples:
                     
 | Boolean | 
| isempty | isempty( variable) | Checks if a given NodeID, String, LocalizedText, or DataTime is empty. | Boolean | 
| if | if( condition, value_if_true, value_if_false) | Checks if the  conditionis true and returns either value_if_trueor value_if_false The syntax must meet these requirements:
                     
 | value_if_truedata type | 
| left_of | left_of(string, pattern) | Returns the substring on the left of the first occurrence of the regular expression pattern.  
     IMPORTANT: 
    Do not use wildcards in patterns. | String | 
| right_of | right_of(string, pattern) | Returns the substring on the right of the first occurrence of the regular expression pattern. 
     IMPORTANT: 
    Do not use wildcards in patterns. | String | 
Output
      The resulting value of the expression.
Examples
      Return the absolute value of a variable

If variable value is higher than 40, toggle the visibility of a graphic object

If variable value is higher than 50, change the background color of a graphic object to blue

If variable value is between 30 and 40, blink the green led object when active

If text box border color is red, enable the button

If the label text equals to "WARNING", change the label text color to red

expression
expression evaluator
    
Provide Feedback
 Read from the source node to the parent.
Read from the source node to the parent. Write from the parent to the source node.
Write from the parent to the source node. Read from the source node to the parent and write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.