Converters
    Use converters to transform the source value and then assign the value to the parent node.
     TIP: 
    If you intend to use a converter and its properties in several complex dynamic links, create a converter type and then use the converter type instances in multiple complex dynamic links. If you intend to use a converter and its properties in a single complex dynamic link, create a local converter.
Converter types and converter instances
      Create converter types and then use instances of converter types in multiple complex dynamic links. See Create a converter type and Create a complex dynamic link.
FactoryTalk Optix Studio
 includes these predefined converter types:
        Local converters
      A local converter is specific to a singular complex dynamic link that you cannot reuse in other complex dynamic links. See Create a complex dynamic link.
Converter example
      An example converter in the complex dynamic link editor may contain:

| Item | Name | Description | 
|---|---|---|
|  | Parent variable | The variable value, which value is the converter output. | 
|  | Dynamic link direction | The direction between the converter output and the converter logic. The direction changes as you select the icon:
                   
 | 
|  |   Insert | Inserts another converter block. | 
|  | Converter name | The name of the converter object. | 
|  | Converter properties | You can set the properties values to:
                   
 | 
|  | Source dynamic link | Either a dynamic link to a variable or tag value or another converter. | 
converter
converter type
converter instance
    
Provide Feedback
 Read from the source node to the parent.
Read from the source node to the parent. Write from the parent to the source node.
Write from the parent to the source node. Read from the source node to the parent and write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.