Manage Controller Communication

The controller provides connection resources whenever communication is established between two devices.
Connections are used when the system contains the following conditions or activities:
  • I/O modules, communication modules, and adapters are present in the I/O configuration of the user project.
  • Produced or consumed tags are configured in the user project.
  • Connected Messages are executed in the user application.
  • External devices, programming terminals, or HMIs communicate with the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal