I clicked Security, but permissions I set up do not take effect

When you right-click an item in the
Explorer
and then select
Security
, the permissions you set up take effect on the item you right-clicked. For example, if you right-click the
Users
or
Computers
folder, select
Security
, and then specify permissions, you are limiting who can access the Users or Computers folder and its contents.
Right-clicking the
Users
folder or the
Computers
folder and then specifying security permissions does not limit a particular user or computer's access to resources in the
FactoryTalk
system. To secure resources, right-click the resource, select
Security
, and then specify security permissions for user and computer accounts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal