Minimum password age policy is not in effect
Possible cause and solution:
- If theMaximum password agepolicy is set less than theMinimum password agepolicy, the minimum password age is ignored, and users are prompted to change their passwords after the maximum password age expires.To correct this problem, setMaximum password ageto a greater value thanMinimum password age.
Provide Feedback