I cannot create, edit, or delete a logical name
Possible cause and solution:
- You do not have the Configure Security permissions required to create a logical name.Contact yourFactoryTalkAdministrator and request the additional permissions.
- Either your computer or theFactoryTalkNetwork Directory Server computer is disconnected from the network.Check the network connection between your computer and theFactoryTalkNetwork Directory Server.
Provide Feedback