I cannot create areas in an application
Possible cause and solution:
- Attempting to edit a local application.If you are editing an application and find that you cannot create areas, check that you are not editing a local application. You cannot create areas in local applications. You can only create areas in network applications.
If you are editing a network application but still cannot create areas, it may be because:
- Your user account has not been granted the appropriate security permissions. Check with your localFactoryTalksystem administrator.
- The computer you are using is not connected to the network directory server or is not connected to the network. Check the computer's connections.
- The network directory server computer is not connected to the network. Check the network directory server connections.
Provide Feedback