I configured the wrong directory
If an error occurred while installing
FactoryTalk Services Platform
, you might have to run the wizard manually to configure the FactoryTalk Directory
. If you do not configure a directory that a software product needs to use, the product will not run. If the product uses both directories and you configure only one of them, some features of the product might be unavailable.If this happens, run the
FactoryTalk Directory
Configuration Wizard again and then configure the correct directory.Provide Feedback