Alarms settings

When Redundancy is enabled,
Alarms settings
on the
OPC UA Servers
tab can only be configured for the primary server. Users can only read the configuration in the Secondary server tab, which is the same configuration as the primary server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal