Things to mind after changing the workstation hostname
To ensure system functionality after renaming the computer hosting the Connector, do the following:
- UpdateClient AddressonOPC UA Serversif the reverse connect is enabled.
- Regenerate the outgoing certificate.The OPC UA Server must trust the new certificate if necessary.
- Verify the hostname onConnector Settingsif you use Localhost to run the Connector.
- Change the computer name in the FactoryTalk network directory. SeeFactoryTalk Services Platform Helpfor more details.
Provide Feedback