Import a certificate

When establishing a connection between an OPC UA Server and
FactoryTalk Linx
OPC UA Connector, the certificates from both sides must be presented and trusted separately.
The user can choose to import an incoming certificate and a custom outgoing certificate manually.
FactoryTalk Linx
OPC UA Connector version 6.20.00 and earlier creates an outgoing certificate by default.
TIP:
Use
Manage Access
to limit access to security certificate management operations to administrators or individuals. This function is only available to Administrator.

To import a certificate

  1. In , select
    Certificate Management
    .
  2. On
    Certificate Management
    , select
    Incoming Certificate
    or
    Outgoing Certificate
    , and then select
    Import
    .
  3. In , select a certificate file with one of the following file extensions, and then select
    OK
    .
    • .pem
    • .cer
    • .crt
    • .der
    • .p7b
    • .p7c
    • .p12
    • .pfx
  4. (optional) If an outgoing certificate requires a password to decrypt, enter the correct password to continue.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal