Device counters
The following are the device counter's parameters and their meanings. These counters are associated with the service configuration.
Parameter | Description | Type |
---|---|---|
Address | Shows the device address, such as IPv4, hostname, or DNS. | Text |
AliasName | Shows the device address's alias name. This counter is the user-assigned name for the device that is set in the configuration in FactoryTalk Administration Console. | Text |
ConnectionStatusCode | Shows the connection status code.
The code is returned by the Windows ICMP service. | Numeric |
LastPingAttemptTime | Shows the last attempt time to ping the device. For example: 2024-8-8 16:08:48.5293961 | String |
LastPingFailureTime | Shows the last failure time to ping the device. For example: 2024-8-8 16:08:48.5293961 | String |
LastPingSuccessTime | Shows the last success time to ping the device. For example: 2024-8-8 16:08:48.5293961 | String |
PingDiagnosticReset | Resets the device counter. Once a client is connected to the FactoryTalk Resource and Status server, you can change the PingDiagnosticReset value to 1 to reset these device counters, and then the service will reset the value to 0 automatically:
| Bool |
PingQuantityAttempts | Shows the attempts number of pinging devices. | Numeric |
PingQuantityFailures | Shows the failure number of pinging devices. | Numeric |
PingQuantitySuccess | Shows the success number of ping devices. | Numeric |
RefreshPingStatus | Starts a data update cycle immediately. | Bool |
Provide Feedback