Status code
The following are the address' status codes and their meanings. The code is returned by the Windows ICMP service. For more information, see ICMP_ECHO_REPLY (ipexport.h) - Win32 apps | Microsoft Learn.
Status code | Value | Meaning |
---|---|---|
IP_SUCCESS | 0 | The status was success. |
IP_BUF_TOO_SMALL | 11001 | The reply buffer was too small. |
IP_DEST_NET_UNREACHABLE | 11002 | The destination network was unreachable. |
IP_DEST_HOST_UNREACHABLE | 11003 | The destination host was unreachable. |
IP_DEST_PROT_UNREACHABLE | 11004 | The destination protocol was unreachable. |
IP_DEST_PORT_UNREACHABLE | 11005 | The destination port was unreachable. |
IP_NO_RESOURCES | 11006 | Insufficient IP resources were available. |
IP_BAD_OPTION | 11007 | A bad IP option was specified. |
IP_HW_ERROR | 11008 | A hardware error occurred. |
IP_PACKET_TOO_BIG | 11009 | The packet was too big. |
IP_REQ_TIMED_OUT | 11010 | The request timed out. |
IP_BAD_REQ | 11011 | It was a bad request. |
IP_BAD_ROUTE | 11012 | It was a bad route. |
IP_TTL_EXPIRED_TRANSIT | 11013 | The time to live (TTL) expired in transit. |
IP_TTL_EXPIRED_REASSEM | 11014 | The time to live expired during fragment reassembly. |
IP_PARAM_PROBLEM | 11015 | It was a parameter problem. |
IP_SOURCE_QUENCH | 11016 | Datagrams are arriving too fast to be processed and datagrams may have been discarded. |
IP_OPTION_TOO_BIG | 11017 | An IP option was too big. |
IP_BAD_DESTINATION | 11018 | It was a bad destination. |
IP_GENERAL_FAILURE | 11050 | It was a general failure. This error can be returned for some malformed ICMP packets. |
Provide Feedback