Feature security properties
The following table shows the relationship between FactoryTalk Resource and Status feature security policies and securable actions that the user can perform:
Feature security policy | Allow | Deny |
---|---|---|
View Configurations | Allow users to view the FactoryTalk Resource and Status server configurations. | Hide the FactoryTalk Resource and Status server configurations. |
Modify Configurations | Allow users to edit the FactoryTalk Resource and Status server configurations. | Set the FactoryTalk Resource and Status server configurations as read-only. |
Provide Feedback