Troubleshoot the DeviceNet configuration
There are three main steps in troubleshooting problems with a DeviceNet I/O configuration:
- Check the basics
- Check the slave device's configuration
- Check the scanner device's configuration
Perform these steps in the order shown. Refer to the links below for these procedures.
If the actions above do not correct the problem, then check the
FactoryTalk View ME
configuration.Provide Feedback