Secure FactoryTalk Linx with FactoryTalk Security
Use
FactoryTalk Security
to secure FactoryTalk Linx
by improving the security of an automation system by limiting user access. FactoryTalk Security
authenticates user identities and authorizes user requests to access a FactoryTalk
-enabled system. These security services are fully integrated into the FactoryTalk Directory
and are included as part of the FactoryTalk Services Platform
that installs with many products.Provide Feedback