Compare FactoryTalk Linx to RSLinx Classic
The following are some differences between
FactoryTalk Linx
and RSLinx Classic
:- InFactoryTalk Linx, if a station is not found during a browse, it does not appear on the display, regardless of whether or not that station was previously discovered. This contrastsRSLinx Classicred X approach of highlighting a station that was previously discovered, but is no longer present.
- In comparison toRSLinx Classic,FactoryTalk Linxis optimized forControlLogixcommunications, and provides a more focused set of available communication drivers and routing options.
- InFactoryTalk Linx, a device shortcut represents a name that stands for the device you want to connect to, the data that the device contains, and the communication path associated with that device. This is similar to DDE and OPC topics inRSLinx Classic. However, withRSLinx Classic, all applications see and use the same topics. WithFactoryTalk Linx, each application has its own shortcuts.
- When a Boolean value is read into an integer usingFactoryTalk Linx, it is represented as 0 or -1. When a Boolean value is read into an integer usingRSLinx Classic, it is represented as 0 or 1.
Provide Feedback