When I browse my Ethernet, why do some of my devices not display?

Some older Ethernet-based industrial devices do not support the service that
FactoryTalk Linx
uses to browse the Ethernet. To rectify the situation, right-click the network and click
Add Device
to manually add the devices to the workstation’s Ethernet network.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal