Why does my backplane have an address?
The address shown on the backplane property page is actually the address of the ENB/CNB consumed on the backplane. The ENB/CNB is shown as the parent of the chassis, and it is not shown again as a child of the chassis.
Provide Feedback