What if I accidentally delete my network from the communications tree?
If you use the communications tree to delete a network in the topology (that is,
right-click
on a bridge device and select Delete
), you cannot recover the network by re-browsing.If you delete a network from your topology, you can restore it by deleting the parent device of the deleted network, and then re-browsing the network.
If the parent device is not a physical device and was added to the topology manually, then you will need to restore the device and network manually.
Provide Feedback