Add an alias (ControlNet I/O)
After adding an address block and a connection, you may add an alias to a data point in your local ControlNet configuration.
To add an alias to a data point in your (local) ControlNet configuration
- From theCommunication Setupeditor,right-clickon the ControlNet scanner and clickProperties.
- Click theI/O Configurationtab.
- Click+to expand the scanner.
- Click+on eitherInputorOutputto view its address blocks and their respective connections.
- Right-clickonInputs, then clickAdd Aliasto display theAlias Propertiesdialog box.
- Enter a uniqueNamefor the data point. Names are case-insensitive, have a maximum of 254 characters, and can use any character except: @, :, /, [, ], ., comma, or space.
- Choose theAlias Data Type.Note that the Alias Data Type selected affects the options available on the Alias Properties dialog box. Refer to the links at the end of this topic for detailed information.
- Specify theStart Wordof the data point.TIP:No validation checking is performed to ensure you have not initialized an overlapped variable with a different value somewhere else.
- ClickOverlapsto display theAddress,Type, andAlias Nameof any overlapping aliases.TIP:The RIO configuration tool does not ensure that you have not configured overlapping aliases.
- When you are finished, clickOKto close theAlias Propertiesdialog box.IMPORTANT:A value of 0 is assigned to any bit in the output table whose value has not been user-specified. Therefore, if an output alias does not have an initial value specified, or if an alias has not been defined for an area of the output table, a value of 0 is assigned to it, and a warning message will be displayed. However, the ControlNet Scanner is still able to enter run mode. You must be aware of the effect this may have on the output devices in your application since a value of 0 is applied immediately when the ControlNet Scanner goes into run mode.
Provide Feedback