Create and test a FactoryTalk View ME application
The steps shown here provide an overview of an example showing how to create and test a graphic display that will read a single data point tag from a target controller on an Ethernet network. This process creates the topology data that specifies the location of the target controller from which you want to read data.
This example shows how to read data from an L1 controller.
To create and test a
FactoryTalk View ME
application using FactoryTalk Linx
(overview)- Create a newFactoryTalk View MEapplication (example)
- Browse for the target controller inFactoryTalk Linx(example)
- Define a shortcut to the device (example)
- Create a numeric control that references data in the device (example)
Provide Feedback