Communications tab

The
Communications
tab shows a view of the system that is rooted from this workstation. It reflects the view of the topology from the
FactoryTalk Linx
server on this workstation.
TIP:
Use the drop-down list in this tab to switch between
FactoryTalk Linx
Instance01 Server and
FactoryTalk Linx
Instance02 Server driver topology tree.
Local
FactoryTalk View SE
or
FactoryTalk View ME
application doesn't support
FactoryTalk Linx
Instance02 Server.
If you are running
FactoryTalk View ME
, the
Communications
tab shows the same information as the
Design (Local)
tab on the
Communication Setup
editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal