Alarm mail rule configurations

With the SMTP policy configured, you can configure the alarm mail rules. These rules use priority and scope as criteria for email notifications about active alarms within an application. When these alarms are triggered, email notifications containing the alarm details are sent to the designated recipients.
TIP: Alarm emails use the default language of the application.
Use these properties to configure alarm mail rules.
Setting
Description
Email Rules
Plus sign or
Add an email rule
Creates rules.
Overview
Lists all the rules and their properties.
An asterisk (*) indicates that there are unsaved changes.
Rule
Configures rule properties.
An asterisk (*) indicates that there are unsaved changes. A warning icon indicates that invalid recipient email address. A stopped icon indicates that the rule is disabled. A recycle bin icon allows you to delete the rule.
Overview
pane
Read-only properties
Shows the properties of each rule.
Recipient emails highlighted in red means they are not valid.
Edit button
Goes to the rule properties pane for you to edit.
Rule properties pane
Name
Sets the name of the rule.
Description
(optional) Sets the description of the rule.
Disable this rule
Disables the current rule. This check box is cleared by default.
If you decide to reactivate a disabled rule, clear this check box. All the properties are retained.
Alarm Priority
Sets the alarm priorities for triggering email notifications.
By default, alarms of all priorities can trigger notifications.
Alarm Scopes
Sets the alarm scope for triggering email notifications.
By default, alarms of all scopes can trigger email notifications.
RECIPIENTS
Sets the recipients who will receive email notifications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal