Define system-wide severity settings

Use the
Policy Settings
tab in the
Severity Settings Properties
dialog box to specify:
  • Severity settings that apply to controller status alarms generated by
    FactoryTalk Linx
    .
  • Tracking events that are logged as audit messages when an operator interacts with an alarm.
To change severity settings for individual alarms, use the
Logix Designer
application for device-based alarms, the Alarm and Event Setup editor on the Tag Alarm and Event server for tag-based alarms, or the
FactoryTalk Linx
OPC UA Connector for OPC UA alarms.
To define system-wide severity settings
  1. Open
    FactoryTalk Administration Console
    or
    FactoryTalk View Studio
    .
  2. In the
    FactoryTalk
    Explorer window, expand
    System > Policies > System Policies >
    FactoryTalk Alarms and Events
    .
  3. Double-click
    Severity Settings
    .
  4. Define system-wide severity settings as needed.
  5. When you are finished making changes, click
    OK
    to close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal