Start FactoryTalk Alarms and Events Database Update Utility
FactoryTalk Alarms and Events
Database Update Utility is automatically installed along with FactoryTalk Alarms and Events
when you install FactoryTalk View SE
.To start
FactoryTalk Alarms and Events
Database Update Utility- SelectStart > All Programs > Rockwell Software > FactoryTalk Alarms and Events > FTAE Database Update Utility.
- In theConnect to Serverdialog box, enter the following information:
- Server nameThe name of theMicrosoftSQL Serverinstance. It must be the name of a server on the network, an IP address, or the name of theSQL ServerConfiguration Manger alias.
- User nameA validSQL Serveraccount.TIP:Make sure to log on with an existing database user name that associated with the database whose tables you want to merge.
- PasswordThe password of the account.
- (optional) Configure sign-in options.Encrypt connectionForces encryption of the connection.Trust server certificate
- IfEncrypt connectionis selected:
- WhenTrust server certificateis cleared, the HMI server or alarms and events server starts the certificate handshake process to validate the certificate on the SQL Server computer. If the certificate is not present or if the validation of the certificate fails, the connection is closed.For more information, see Configure the certificate for encrypted connection to the database.Important: In cases where theTrust server certificatesetting is cleared, if SQL Server is used for FactoryTalk View SE data grids, you must configure the certificate for the HMI server. If SQL Server is used for alarms and events, you must configure the certificate for the alarms and events server.
- WhenTrust server certificateis selected, the HMI server or alarms and events server does not validate the certificate on the SQL Server computer.
- IfEncrypt connectionis cleared, theTrust server certificatesetting is ignored.
- ClickLog on.
Provide Feedback